An Overview of Audio Products
Audio products: A device that records, reproduces, and processes sound, allowing transmission to the listener.
What are Vibration Motors?
A vibration motor is a compact device that creates motion in a specific direction through the use of an unbalanced mass rotating on a motor shaft.
How do Audio Products work?
Let's take the example of the Condenser Microphone in terms of Audio products and how condenser mics work mainly depending on the capacitor inside. The capacitor consists of two metal plates, one in the front and another in the back, with which there is a voltage in between. One of the metal places called the back plate is typically made out of solid brass and the other is called the diaphragm made of lightweight metal. The capacitor is housed in a microphone capsule. The front plate detects subtle vibrations in air pressure when sound is being recorded. The diaphragm inside Audio products feels the vibration, and the distance between the diaphragm and the back plate makes the voltage change. The voltage is an electrical signal that simulates the original sound waves.
What are the Advantages of Vibration Motors?
1. Vibration motors are considerably small and lightweight, making them suitable for portable devices.
2. Vibration motors are relatively cheap, making them a cost-effective solution for many applications.
3. There is a wide range of applications for Vibration Motors.
What are the LCSC Categories of Audio Products and Vibration Motors?
Microphones, Buzzer Plates, Speakers, Vibration Motors, MEMS Microphones, Buzzers