LCSC supplier XUNPU will share the knowledge of the IPEX connector with us. In this article we will understand the definition and structure of the IPEX connector.
IPEX Connector Definition
IPEX connector, also known as MHF connector (Micro Coaxial Connectors), is a micro coaxial connector. It serves in wireless communication modules, antennas, WiFi modules, Bluetooth modules, and other applications in electronic equipment. Its main function is to provide high-frequency and high-speed signal transmission. In small electronic devices such as laptops, smartphones, and tablets, IPEX connectors are mainly used for signal transmission between antennas and motherboards or other circuit boards, such as the transmission of wireless signals such as Wi-Fi, Bluetooth, and GPS. The transmission of wireless signals is critical to the proper functioning of these small electronic devices.
IPEX connector: SP-RF-001
IPEX Connector Structure
The IPEX connector is a miniature coaxial connector whose structure mainly consists of three main parts:
Connector Head: This is the contact part of the connector to mate with the port of the target device. It is usually made of metal to provide stable electrical performance and durability. Connector tips come in many different shapes and sizes to match the ports of different devices.
Cable: A cable is another component of a connector that transmits signals or power. Typically, a person connects one end of the cable to the connector and the other end to the internal circuitry of the electronic device. To ensure stable signal transmission, one usually shields cables to prevent electromagnetic interference.
Accessories: These are optional components that provide additional functionality or enhance the performance of the connector. Common accessories include nuts, screws, adapters, etc., which can secure the connector in place or provide additional attachment points. In addition, the structure of the IPEX connector also includes some other components, such as shells, internal circuits, filters, etc. The role of these components is to provide stable signal transmission and protect the connector from environmental influences.
IPEX connector: SP-RF-003
Overall, IPEX connectors are compact and well-designed, making them a connector type well suited for signal transmission in a variety of electronic devices.
About Manufacturer Xunpu
Xunpu Electronic Technology Co., Ltd. focuses on the R&D and production of connectors and switches! Xunpu’s products include SIM card holder, TF card holder, SD card holder, all-in-one card holder, touch switch, TYPE C connector, USB socket, headset socket, power socket, FPC socket, PCIE socket and other reliable connectors and customized components, which serve in automotive, industrial, Internet of Things, wearable devices, communications, consumer goods and other industries.
LCSC is a global distributor of electronic components. With over 4 million customers, we process about 14,000 orders daily. LCSC is known for quick delivery through in-stock inventory. View and select Xunpu’s products at LCSC.