Nationstar Optoelectronics Launched 817 Optocoupler Device

LCSC supplier, Nationstar Optoelectronics, has introduced a new series of high-quality 817 optocoupler devices. These devices are suitable for a broad spectrum of applications, encompassing power adapters, smart home appliances, electric vehicle chargers, photovoltaic inverters, and more. Their introduction is expected to invigorate the fields of energy storage and new energy applications.

Optocoupler Device

Optocoupler is an electro-optical-electric conversion device that uses light as a medium to transmit electrical signals. It plays a key isolation role in input and output electrical signals. Therefore, it has strict requirements for stability and reliability.

The new 817 optocoupler product from Nationstar Optoelectronic Devices Division has completed CQC, VDE, and UL certifications, demonstrating its reliability and quality.

Optocoupler Product Advantages

The Optoelectronic Devices Division, capitalizing on its strengths, takes a proactive approach in innovating its research and development. They actively refine their processes and work on mastering the key core technologies of optocoupler devices. As a result, they have successfully highlighted the following product advantages:

  1. High process standards: production using automated equipment to ensure product consistency and stability;
  2. Good reliability: It has passed industrial control-level high-standard reliability tests, and the quality is more guaranteed;
  3. Excellent air tightness: independently designed lead frame, optimized frame and colloid combination;
  4. Strong voltage resistance: collector-emitter breakdown voltage BVCEO>80V;
  5. High safety: input-output isolation voltage is up to 5000 Vrms, safer and more reliable.
Optocoupler Product Specifications

To meet the diverse needs of customers, Nationstar Optoelectronics’ 817 series optocoupler products have complete specifications and are suitable for a variety of scene applications.

Optocoupler applications

Optocoupler Product Specifications

At the same time, the business unit is actively extending the optocoupler product line based on the 817 platform. They will launch 815, 851, 852 and other series of products one after another. The pin format covers DIP and SMD and can provide customers with customized products and technical solutions.

In recent years, with the continuous deepening of the innovation-driven development strategy, Nationstar Optoelectronics has broadened its horizons in LED technology. The optoelectronic device division closely monitors market trends and is actively engaged in the development of product updates and iterations. Besides the newly launched optocoupler devices, the company has introduced new products in the field of intelligent sensing, including VCSEL devices and a health sensing series. Additionally, the company offers a diverse range of product configurations in specialized areas such as infrared and ultraviolet LEDs, allowing for the provision of tailored product services to meet market demands. View and select Nationstar’s 817 series optocouplers and other products on LCSC.

Newsletter
Connect with us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30am to 12pm and 1:30pm to 10pm,
Monday through Friday, UTC/GMT +8.

SSL encrypted
payment
© 2024 LCSC.COM All Rights Reserved. 粤ICP备17041818号