Shikues is one of the world’s leading manufacturers of semiconductor discrete components. It mainly provides engineers and designers with various semiconductor products and software for better experience in automotive, communication, computer, consumer electronics, industries, LED lighting, healthcare, aviation, and power applications.
Since its foundation, with the idea of “to have good products equipped with cores” and the tenets of safety, low energy consumption, and high performance, Shikues has devoted itself to the research and development of semiconductor discrete components. What is more, nearly a quarter of employees work in the fields of the research and development and design of products with expenses accounting for about 22% of total revenue. In addition, thanks to the hard work of young, dreamy, and passionate employees, Shikues has made great progress, and its products are exported to North America, Europe, and the Asia-Pacific region, making itself one of the most innovative companies in the semiconductor discrete components industry.
The discrete components product series manufactured by Shikues covers more than 40 subcategories such as diodes, transistors, Schottky, silicon carbide Schottky, gallium nitride IC, lithium battery protection IC, IGBT, ESD protection tubes, rectifiers, MOSFET, etc. It has more than 5,000 items.
Discrete Components Recommendation: DW01
Shikues DW01 is a single-cell rechargeable lithium-ion battery protection integrated circuit. Its performance features include not only low operating current, high-precision overcharge, and over-discharge detection, but also a series of other excellent features.
First, the DW01 has a low operating current of 4uA, which means the product consumes very little energy in standby mode. This is particularly important for electronic products that require long-term standby. It can effectively extend the service life of the battery, reduce the frequency of charging the battery, and improve the endurance of the product.
Secondly, DW01 adopts high-precision overcharge and over-discharge detection functions. The overcharge detection voltage is 4.280V, the over-discharge detection voltage is 2.4V, and the accuracy is ±50mV and ±100mV respectively. This means that discrete components DW01 can accurately monitor the voltage of lithium batteries. Once an abnormal voltage is detected, protection measures will be triggered in time to prevent the battery from overcharging or over-discharging, effectively protecting the safety and stability of the battery.
In addition, DW01 also has an over-current protection function, which can cut off the circuit in time when the current is abnormal to prevent the battery from being damaged. The overcurrent detection voltage is 0.16V, the short-circuit current detection voltage is 1.3V, and the accuracy is ±30mV respectively. This overcurrent protection function can effectively prevent the battery from being damaged by overload under high load conditions, ensuring the safety and reliability of the battery.
LCSC is a global distributor of electronic components. With over 4.6 million customers, we process about 16,000 orders daily. LCSC is known for quick delivery through in-stock inventory. LCSC is the authorized distributor of Shikues. View and select Shikues’s discrete components and more at LCSC.