Unlocking PCB Thermal Management: Enhance with Thermal Relief Pads

The proper design of thermal relief pads optimizes soldering and improves heat management, reducing defects.

However, designers often face challenges in designing and using these pads, as well as selecting the right substrate materials. This article explains the principles and applications of thermal relief pads and introduces our innovative thermoelectric separation copper substrates for efficient thermal management.

Have you ever faced soldering failures due to uneven heat distribution when welding high-power components? – Thermal relief pad design could be your solution.

By properly designing thermal relief pads, you can significantly improve soldering quality, particularly in large copper foil or high-power component applications. This not only solves heat dissipation issues but also optimizes production efficiency.

Basics and Process

What is a Thermal Relief Pad?

A thermal relief pad is a specially designed solder pad connected to large copper foil via copper spokes. This design aims to reduce the rapid loss of heat during the soldering process, ensuring smooth soldering completion.

Comparison of standard pad and thermal pad design, showing how thermal pads reduce heat dissipation during soldering
Comparison of standard pad and thermal pad design, showing how thermal pads reduce heat dissipation during soldering (Image source: online)

Functionality Breakdown:

  • Prevents Excessive Heat Dissipation: The thermal relief pad restricts the heat transfer area between the copper foil and the pad, concentrating the heat for better soldering and avoiding cold or soldering defects caused by rapid heat loss.
  • Protects PCB Structure: Reduces PCB warping or delamination that can occur from large copper foil under high temperatures.

Common Applications: Thermal relief pads are often used in reflow and wave soldering processes for PCB designs requiring high-power transmission, such as power supply modules and LED driver circuits.

Design Solutions: How to Optimize Your PCB for Heat Dissipation?

Optimizing thermal relief pads involves multiple parameters, including pad size, number and width of spokes, and copper foil thickness. These adjustments can greatly impact the heat dissipation performance of the thermal relief pad.

In dual-layer PCB designs, you can effectively control heat conduction paths by planning the number and width of spokes, reducing soldering difficulty, and improving thermal management efficiency.

Comparison of direct connection vs. thermal relief pad design, impact on heat dissipation and solderability
Comparison of direct connection vs. thermal relief pad design, impact on heat dissipation and solderability (Image source: online)

Additionally, copper cladding is another common heat management technique. By utilizing large copper foil as a heat transfer path, heat generated by components is quickly distributed across the entire PCB, with the potential for further dissipation via heatsinks or the chassis.

However, as high-power components become more prevalent, the limitations of traditional copper cladding designs are becoming more apparent. When heat-generating components are concentrated in small areas, copper thickness and thermal conductivity may not meet the demands, leading to localized overheating.

Thermoelectric Separation Copper Substrates: A Thermal Management Solution

Our double-sided copper substrate, compared to traditional single-sided aluminum or copper substrates, adopts a “thermoelectric separation” design. This unique structure enhances thermal conductivity, reaching 380 W/m·K—far exceeding the 1-2 W/m·K of standard copper substrates.

Cross-sectional comparison of standard aluminum/copper substrate vs. thermoelectric separation copper substrate
Cross-sectional comparison of standard aluminum/copper substrate vs. thermoelectric separation copper substrate (Image source: online)
  • Wide Application: This substrate supports both surface-mount and through-hole components.
  • Efficient Heat Dissipation: Particularly suitable for high-power components like transistors, MOSFETs, and LEDs.
Thermoelectric separation copper PCB with physical examples and design for enhanced thermal conductivity
Thermoelectric separation copper PCB with physical examples and design for enhanced thermal conductivity (Image source: online)

Case Study: Thermal Management Optimization in LED Driver Circuits

In a recent LED driver circuit project, we used double-sided copper substrates. This material increased the circuit board’s heat dissipation by 40%, much like adding a more efficient heatsink to the PCB. This reduction in heat-induced stress on the board’s surface also extended the device’s lifespan.

Example of PCB using double-sided copper substrate for enhanced heat dissipation in LED driver circuit
Example of PCB using double-sided copper substrate for enhanced heat dissipation in LED driver circuit (Image source: online)
Example of PCB using double-sided copper substrate for enhanced heat dissipation in LED driver circuit
Example of PCB using double-sided copper substrate for enhanced heat dissipation in LED driver circuit (Image source: online)

Service Advantages: Exceptional Thermal Management Solutions for Optimized Product Performance

As a leading PCB & PCBA manufacturer, LCSC is dedicated to offering efficient and reliable thermal management solutions. We offer two unique substrate categories to provide optimal support for your high-heat applications:

Aluminum Substrate:

  • Excellent thermal conductivity and electrical insulation properties, ideal for LED driver circuits and other high-heat applications.
  • Stable and reliable, controlling component temperature rise and improving system reliability and lifespan.
Aluminum substrate with excellent thermal conductivity and electrical insulation
Aluminum substrate with excellent thermal conductivity and electrical insulation (Image source: online)

Copper Substrate:

  • Exceptional thermal conductivity and heat dissipation, especially suitable for high-power supplies, LED lighting, and power semiconductors.
  • Support complex design, combining thermal performance with structural stability for complex multilayer designs.
Copper substrate with exceptional thermal conductivity and heat dissipation
Copper substrate with exceptional thermal conductivity and heat dissipation (Image source: online)

Some images are sourced online. Please contact us for removal if any copyright concerns arise.


Custom Cables: Save 50%+ Avg Cost By JST, Molex, TE Alternatives | Processing Fee Down to $1 Per Piece | No Minimum Order Quantity (MOQ) Required

PCB & PCBA: New Customer Get Coupons Up to $125 | 1 – 32 Layers From $2 /5pcs | PCB Assembly From $8 /5pcs

Front Panels: High-quality Front Panel Acrylic/PET | Front Panel Order Up to 30% Off | Membrane Switch Available Soon

More Discount Information
Connect With Us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30 am - 12 am, 1:30 pm - 10 pm
Monday - Friday, UTC/GMT +8
View Our Social Channels
Encrypted
Payment
© 2025 LCSC.COM All Rights Reserved.
粤ICP备17041818号 ISO/IEC