MDD High Current 6A/8A Bridge Rectifier

A full bridge rectifier consists of four diodes and has four pins. The connection point of the negative poles of the two diodes is the “positive pole” of the DC output end of the full bridge rectifier. Similarly, the connection point of the positive poles of the two diodes is the “negative pole” of the DC output end of the full bridge rectifier.

MDD·TTF Series Patch Bridge Rectifier

As electronic device chargers become more compatible and charge faster, their power also increases. However, maintaining portability requires the charger to be compact, which means the full bridge rectifier needs to pass a larger current within a limited space. In order to improve production efficiency, there are requirements for chip full bridge rectifiers. Under these circumstances, MDD has launched the TTF series of chip full bridge rectifiers.

MDD TTF Package Bridge Rectifier: The Maximum Current Can Be 8A, 6A, 4A. ​

The MDD TTF bridge is an SMD full bridge rectifier that can replace the GBU810 8A, 1000V bridge rectifier. It’s an excellent alternative to the large and labor-intensive direct plug-in bridge rectifiers such as GBL, GBP, and GBU.

MDD TTF Package Bridge Rectifier Model:
TYPE NO. MARKING Max.Reverse Voltage Max.Aver. Rect.Current Peak Fwd.
Surge Current
                Max.Fwd.Voltage
@25℃&Rated lo
VRM (V) lo(A) IFSM(A) Rated lo(A) VF(V)
TT4MF TT4MF 1000 4 150 4 0.83
TT6MF TT6MF 1000 6 200 6 1.0
TT8MF TT8MF 1000 8 220 8 1.0
TTR4MF 1000 4.0 150 4.0 0.95
TTR5MF 1000 5.0 180 5.0 1.1
TTR6MF 1000 6.0 200 6.0 1.0
TTR8MF 1000 8.0 220 8.0 1.1
Features of MDD TTF Package Series Bridge Rectifier
  • Halogen-free type.
  • Built-in glass passivated rectifier chip structure.
  • Comply with RoHS product requirements.
  • Low power loss and high efficiency.
  • High current capability.
  • Plastic flame retardant grade 94V-0.
  • This package can be shared with Z4GP, TT, and LSB Pad Layouts.
  • Compared to the UMSB package, it features a larger frame and chip with better heat dissipation.
Application Scenarios of MDD TTF Encapsulation

MDD TTF package series full bridge rectifier is Suitable for low-power instruments, household appliances, AC/DC power supplies, and 65W fast charging source adapters.

About MDD

Microdiode Electronics (Shenzhen) Co., Ltd (MDD) is a national high-tech enterprise focusing on the R&D, packaging, testing, and sales of semiconductor power devices.

MDD has been deeply engaged in the semiconductor industry for 15 years. The company always adheres to the product technology as driver and customer needs as core to create a full range of MOSFET, diode, transistor,  bridge rectifier, SiC, etc. Its products cater to industries like new energy vehicles, industrial control, consumer electronics, communications, home appliances, medical equipment, lighting, security, and instrumentation. MDD has served more than 40 countries and regions around the world.

Newsletter
Connect with us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30am to 12pm and 1:30pm to 10pm,
Monday through Friday, UTC/GMT +8.

SSL encrypted
payment
© 2024 LCSC.COM All Rights Reserved. 粤ICP备17041818号