Ai-Thinker, Leading Manufacturer of IoT Wireless Modules

Ai-Thinker Technology is a leading manufacturer of IoT wireless modules (including Bluetooth module and wifi modules) , with a team of over 100 engineers and a factory covering an area of 3000 square meters. It also has a professional RF laboratory for OTA and electromagnetic compatibility (EMC) testing. Ai-Thinker’s product range includes IoT wifi modules, 2.4G modules, LoRa modules, GPRS+GPS modules, bluetooth(BLE) module, Zigbee modules, and NB-IoT mudules, etc.

Ai-Thinker Technology has created Bluetooth modules for Internet of Things(IoT). The PB and TB series are the main Ai-Thinker bluetooth module sold at LCSC Electronics. These Bluetooth module conform to BLE and SIG mesh specifications. Smart lamps, plugs, air conditioners, and other home appliances extensively utilize Ai-Thinker’s bluetooth module.

Ai-Thinker Bluetooth mudules PB-03M
Ai-Thinker bluetooth module PB-03M
Ai-thinker’s Bluetooth module has the following features:
  1. The product Supports the latest Bluetooth BLE 5.2 protocols. It also supports SIG Mesh, Tmall Genie APP voice control, and Amazon Alexa Echo audio control.
  2. Ai-thinker’s product Supports half-hole pad, antenna hole, and onboard antenna. The half-hole pad can guide the antenna to the main board, and the antenna hole allows for direct soldering of the spring antenna onto the module.
  3. The brightness adjustment range (duty cycle) is 5% – 100%, with a PWM output frequency of 1 kHz.
  4. The ESP32-G Bluetooth gateway supports remote control from anywhere, at any time.
  5. Bluetooth module support the secondary development of the SDK in the Windows environment, open source all source codes, and provide support for AT command access to Tmall Genie.
  6. Supports control of Android/iOS apps and WeChat mini-programs.

Ai-Thinker’s line of WIFI modules include the Ai-WB2, RTL87XX, Tmall Elf TG, HiSilicon Hi, Ai-WB1, and ESP8266 series. All wifi module series have received FCC/CE/SRRC/RoHS/REACH certification, with some passing the double 85 test. In addition, the pulling distance test shows that the longest range a module can reach is 500 meters. FLASH memory ranges from 1 to 16 MB. TG/Hi series modules can connect to Tmall Elf or the Huawei ecosystem. The wifi modules are reliable and stable. Ai-Thinker assures customers that all wifi modules have undergone RF, IO communication, and other tests.

Ai-Thinker WIFI Ai-WB2
Ai-Thinker WIFI modules Ai-WB2

LCSC electronics is an international electronic components distributor. Choose Ai-thinker’s Bluetooth and WiFi module at LCSC electronics. 

>>> Bluetooth Modules | WiFi Modules | IoT/Communication Modules | LCSC

Newsletter
Connect with us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30am to 12pm and 1:30pm to 10pm,
Monday through Friday, UTC/GMT +8.

SSL encrypted
payment
© 2024 LCSC.COM All Rights Reserved. 粤ICP备17041818号