Component Layout Optimization: LCSC’s Approach to Reducing Soldering Defects in PCBA

In the electronic manufacturing industry today, the layout of components on a Printed Circuit Board Assembly (PCBA) directly affects product performance, manufacturability, and reliability. As Surface Mount Technology (SMT) progresses toward higher density and finer pitch, a proper component layout becomes crucial to ensuring product quality. This article will delve into the significance of PCBA component layout, analyze the potential issues caused by improper layout, and introduce effective methods for detection and optimization.

The Importance of Minimum Spacing Design and Key Considerations

1.  Correlation Between Minimum Spacing and Stencil Design Apertures

The design of the minimum spacing between components is closely related to the stencil apertures. When the stencil apertures are too large, the stencil thickness is excessive, or the tension is insufficient, deformation can occur. This can lead to misalignment during soldering, resulting in issues such as solder bridging or short circuits between components.

A proper stencil and its apertures
A proper stencil and its apertures (Image source: online)

Key points to consider in the design process to avoid soldering defects:

  • For devices with fine-pitch pins (pin pitch less than 0.4mm), a thinner stencil, typically around 0.08mm, is used to prevent excessive solder paste on the pads, which could lead to solder bridging.
  • For Wi-Fi module components, which require a larger amount of solder paste, typically use a stencil thickness of 0.12–0.15mm, with enlarged stencil apertures.
  • For a PCB contains both scenarios above, a step stencil design can be used to ensure soldering quality.
Several Stencils in one single board
Several Stencils in one single board (Image source: online)

2. The Space Requirements for Operations

Throughout the entire PCBA production process, from hand soldering, selective soldering, tooling, rework, inspection, testing, to assembly, sufficient operational space is required at each stage. For example, hand soldering requires enough space to maneuver the soldering iron, while rework requires easy access for disassembly and component replacement. Therefore, when designing the component layout, these operations must be fully considered, and the spacing between components should be reasonably planned to ensure that each step can be carried out smoothly.

Soldering in operations
Soldering in operations (Image source: online)

3. Relationship Between SMD Component Spacing and Pad Design

The spacing design of surface-mount devices (SMDs) directly affects the pad layout and soldering quality. If the pads do not extend beyond the component’s package, solder paste may climb along the edges of the component’s termination area. This phenomenon is more likely to cause solder bridging and short circuits, especially when the component is thin.

solder climb is poor if the pad design is too small
solder climb is poor if the pad design is too small (Image source: online)
solder climb is poor if the pad design is too small
solder climb is poor if the pad design is too small (Image source: online)
Solder climb is poor if the pad design is too small
As shown in the figure, solder climb is poor if the pad design is too small. (Image source: online)

Therefore, when designing the pads, it is essential to consider the component type and size to ensure the pads extend sufficiently, improving soldering quality. Additionally, adequate safety spacing between surface-mount devices should be maintained to prevent short circuits or other soldering defects caused by insufficient spacing.

The correct pad design, with the pads extending beyond the component package, providing space for solder climb
The correct pad design, with the pads extending beyond the component package, providing space for solder climb (Image source: online)
The correct pad design, with the pads extending beyond the component package, providing space for solder climb.
The figure shows the correct pad design, with the pads extending beyond the component package, providing space for solder climb. (Image source: online)

4. Definition and Influencing Factors of Component Spacing Safety Value

The safety margin for component spacing is not a fixed, absolute value. The spacing is influenced by manufacturing equipment and assembly capabilities. Different manufacturing equipment may vary in precision and stability, and the level of refinement in the assembly process also differs.

Therefore, the safety margin for spacing should consider factors such as severity, likelihood, and safety. In actual design, the minimum spacing between components should be reasonably determined based on specific production conditions and product requirements. They ensure reliable assembly in various manufacturing environments.

Case Study: Practical Applications in Design Optimization

The RK3566-Linux development board employs a precise component layout strategy:

  • Spacing Control of SMD Resistors and Capacitors: The 70mm x 45mm board, smaller than a credit card, prevents soldering short circuits while ensuring signal integrity.
  • Optimized Layout of Multi-functional Communication Modules: The board features built-in WIFI/BT, HDMI, and other modules. The spacing and pad design are perfectly matched, and step stencil technology is used to achieve flawless soldering results. It also includes 14 peripheral interfaces, 500 components, and 79 expansion interfaces.

Our LCSC PCBA service helps customers efficiently transition from prototype design to mass production. It provides one-stop solutions for component procurement, manufacturing, and quality testing

Rear view of the RK3566-Linux development board (Image source: online)

Some images are sourced online. Please contact us for removal if any copyright concerns arise.


Custom Cables: Save 50%+ Avg Cost By JST, Molex, TE Alternatives | Processing Fee Down to $1 Per Piece | No Minimum Order Quantity (MOQ) Required

PCB & PCBA: New Customer Get Coupons Up to $125 | 1 – 32 Layers From $2 /5pcs | PCB Assembly From $8 /5pcs

Front Panels: High-quality Front Panel Acylic/PET | Front Panel Order Up to 30% Off | Membrane Switch Available Soon

Newsletter
Connect with us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30am to 12pm and 1:30pm to 10pm,
Monday through Friday, UTC/GMT +8.

SSL encrypted
payment
© 2024 LCSC.COM All Rights Reserved. 粤ICP备17041818号