Crystal Oscillators for Energy Storage Application

As the global demand for energy storage products grows, the need for efficient, robust, and reliable systems also increases. The demand for frequency device technology has also risen accordingly. With the development of battery energy storage systems with larger capacities, the requirements for parameters such as the maximum allowable current of crystal oscillators are also increasing. Lower excitation and water resistance losses offer two significant benefits. It reduces the cost of energy storage and improves stability under harsh climatic conditions.

Crystal Oscillators Components for Energy Storage Products

Power electronics is a crucial technology for achieving efficient electrical energy storage. Energy storage systems must operate safely and reliably for 20 years. Therefore, the crystal must operate with low losses and provide maximum reliability over a wide temperature range at the lowest possible cost.

Crystal Oscillators Solution

The crystal oscillators used in the application should meet the following conditions:

High stability: 

The frequency accuracy on the PCB needs to be ≤±10PPM to make it more stable and reliable.

Low power consumption:

The crystal oscillator has low power consumption due to its low internal resistance. For example, the 3225-8MHZ crystal oscillator has an internal resistance of ≤150Ω. Crystal oscillators can operate at a lower excitation level.

T/C changes: 

The usage scenarios of energy storage products vary greatly. Therefore, the stability of the crystal oscillator requires the operating temperature range to be -40℃~+85℃ and must be at ≤20PPM.

Crystal Oscillators for energy storage
Crystal Oscillators Selection 

Common frequencies include 5032-8MHz, 3225-8MHz, 12MHz, 24MHz series products.

1: Comply with RoHS and REACH standards, green, environmentally friendly (carbon-reducing) and cost-effective.

2: Accelerate SMT processing capacity with SMT packaging.

3: T/C value performance is better and can reach an industrial level.

4: The product has a long development cycle, which allows for early program development and design.

About Supplier Yajingxin

Founded in 1996, Shenzhen Yajingxin Electronics Co., Ltd. specializes in quartz crystal resonators, filters, and oscillators. The company has two production plants equipped with standardized and dust-free purification workshops. Yajingxin passed ISO 9001:2015 quality system certification and ISO 14001:2015 environmental management system certification. The products serve in high-tech fields such as wireless communications, Internet of Things, vehicle charging systems, timing line control, computer fields, digital products, remote control systems, etc. The products sell well all over the world. The company has become a leader in the industry with its abundant crystal product output and product specifications.

LCSC Electronics is a global distributor of electronic components, offering over 500,000 inventory parts from more than 2,600 suppliers. Customers rely on LCSC for fast delivery due to our in-stock inventory and 130,000㎡ intelligent warehouses. Designers and buyers can find products in design and production quantities at LCSC Electronics. We are the authorized distributor of Yajingxin and offer their crystal oscillators and other products.

Newsletter
Connect with us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30am to 12pm and 1:30pm to 10pm,
Monday through Friday, UTC/GMT +8.

SSL encrypted
payment
© 2024 LCSC.COM All Rights Reserved. 粤ICP备17041818号