Introduction to Ai-Thinker LoRa Module

This week, LCSC electronics supplier Ai-Thinker shared an introduction to their LoRa module. The article will provide the basics of the LoRa module and Ai-Thinker’s featured products.

Due to its ultra-long transmission distance and low power consumption, LoRa technology has broad application prospects in the Internet of Things. LoRa technology finds widespread and successful applications in many fields, such as smart buildings, intelligent industrial parks, asset tracking, smart agriculture, and livestock management.

Ai-Thinker has a wide range of LoRa series, LoRaWAN series, LoRa gateway, and other products. 

Introduction to the Ai-Thinker LoRa Module

LoRa is a wireless communication technology developed by Semtech that can propagate farther than other wireless methods under the same power consumption conditions. It is a new communication technology that can achieve long distance, long battery life, low power consumption, high sensitivity, large system capacity, and broad coverage.

Ai-Thinker LoRa Module Series Products Comparison

Ai-Thinker LoRa module series product

Select Ai-Thinker LoRa Module

Ai-Thinker LoRa Module Ra-01H

aithinker Lora module ra-01h

The current received is 12.15 mA, while the standby current is 1.6 mA. The maximum transmit power is +20dBm, and the maximum operating current is 105mA. Additionally, the receiving sensitivity is -140dBm.

Ai-Thinker LoRa module features:
  • LoRa™ modem.
  • Support FSK 、GFSK、MSK、GMSK、LoRa and OOK mode.
  • Support 803/930MHz.
  • The device operates at a voltage of 3.3V, with a maximum output of 19dBm and a maximum output current of 105mA.
  • Low Power Consumption in a received stat, the received current is 12.5mA, and the standby current is 1.6mA.
  • High sensitivity: as low as 140dBm.
  • Small volume dual-row stamp-hole patch package
  • SPI interface using half-duplex communication, with CRC up to 256-byte packet engine.
Application areas: 

Wireless smoke detectors

Environmental monitoring

Smart meter reading

Smart agriculture

LoRaWAN Module Series Ra-08/Ra-08H
Product advantages:
  • Comes with MCU and can run independently;
  • Transmit power up to +22dBm;
  • Receiving sensitivity-138dBm @SF12/125KHz;
  • Spreading factors fully support SF5/SF6/SF7/SF8/SF9/SF10/SF11/SF12;
  • Supports LoRaWAN and LinkWAN protocols;
  • There are two different versions: low frequency and high frequency;
  • The actual pulling distance test can reach 4.6KM;
  • Mainly promotes meters, smart agriculture and animal husbandry, intelligent cities, street light control, battery-powered sensors, industrial automation, and other fields.
Main functions and parameters
Power consumption/acceptance sensitivity

The Ra-08 module has a transmit power consumption of 115mA at full load, a maximum transmit power of +22dBm, a receiving working current of 6mA and a sleep mode of 1.3uA. Additionally, it has a receiving sensitivity of -138dBm, making it capable of operating normally even in complex interference environments.

The Ra-08H module has a transmit power consumption of 115mA at full load, a maximum transmit power of +22dBm, a receiving working current of 9.5mA and a sleep mode of 1.3uA. Additionally, it has a receiving sensitivity of -138dBm and strong anti-interference ability, allowing it to operate in complex and interference-prone environments. 

Antenna form

The Ra-08 and Ra-08H modules are compatible with various antenna connection methods, including half-hole pads, through-hole pads (requiring soldering), and IPEX sockets. They also support multiple solutions for antenna selection.

Communication distance

The transmission distance of Ra-08 and Ra-08H modules with suction cup antenna is about 4.8km.

Network access method

These modules support two network access methods: OTAA and ABP.

Accessible to the ecosystem

The Ai-Thinker Ra-08H module can connect to TTN servers to facilitate data sending and receiving.

LoRa Gateway Series RG-02

RG-02 is an indoor LoRaWAN gateway. It supports Semtech packet transponder and LoRaWAN base station functions and is compatible with the standard LoRaWAN protocol. It adopts mainstream LoRa modulation and demodulation chip solutions (high-frequency version: SX1302+2*SX1250, low-frequency version: SX1301+2*SX1257). Additionally, it supports ten programmable parallel demodulation paths.

The gateway supports Wi-Fi, Ethernet, and 3G/4G cellular network access. We can deploy it to various application sites. RG-02 is preset with multiple standard LoRaWAN frequency band options, which can adapt to different countries and regions. It also supports user-defined frequency bands to build private LoRa networks.RG-02 can communicate with ABP LoRaWAN end nodes without a LoRaWAN server. The lightweight deployment method is very convenient for system integrators to directly connect it to existing IoT applications without building a LoRaWAN server or using a third-party LoRaWAN Serve.

LCSC is the authorized distributor of Ai-Thinker. And LCSC is a global distributor with an extensive selection of electronic components. LCSC electronics is known to customers for offering in-stock inventory for fast delivery since LCSC owns 130,000㎡ intelligent warehouses. Select Ai-Thinkers LoRa module products at LCSC Electronics.

Newsletter
Connect with us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30am to 12pm and 1:30pm to 10pm,
Monday through Friday, UTC/GMT +8.

SSL encrypted
payment
© 2024 LCSC.COM All Rights Reserved. 粤ICP备17041818号