Based on the GD32F450ZGT6, the LCSC Liangshan development board is an open source development board. It has complete supporting video tutorials, document tutorials, and experimental cases. It provides an online compiler for a quick start in 10 minutes. Open source technology iteration and project-based learning make learning more in-depth and creativity sublimated.
LCSC Liangshan Development Board Background
Origin
The development board is a project with almost no pain points. Why does the JLC group want to enter this niche market? Since software development is more attractive than hardware development, the learning cost is low (one computer can dominate the world), and the market demand is also high. It has caused more and more people to turn to software development. Hardware is the carrier of software, and the entire ecosystem of JLC relies on the group of hardware engineers. We hope to do something for this potential family. Thus, this project was born.
Why Choose the High-end GD32 as the Main Controller?
We have tried many solutions. Eventually, we used the high-end GD32F470ZGT6 chip to prevent performance from limiting everyone’s imagination and innovation.
LCSC Liangshan development board has completed its development, and we are currently troubled with pricing and naming. At that time, global chip prices were on the rise, with many chips experiencing several price changes a day. The GD32 main controller we selected has also been fluctuating around 108 yuan. At this juncture, the founder of the EDA software suggested that we name it the Liangshan. Regardless of price increases or decreases, our development board will be sold for 108 yuan, not aiming to profit from selling boards, but focusing on cultivating engineers as our mission.
Liangshan comes from the novel “Outlaws of the Marsh,” also known as”Water Margin.” It is one of the four classic Chinese classics. The story revolves around 108 outlaws and rebels who gather at Mount Liang (Liangshan) to form a formidable army.
Problems that LCSC Liangshan Development Board Can Solve
- Humanized design with rich expansion interfaces, greatly expands playability and usability. It uses GD32 series chips with powerful performance.
- On the premise of ensuring practical functions, LCSC Liangshan development board is designed to be miniaturized, easy to carry, and suitable for project expansion. It can be used in electronic design competitions and similar events.
- It solves the problem of beginners who are getting started with development boards. There are not many development board tutorial cases used, and they cannot directly apply them to project development after learning.
- Highly cost-effective and high-quality, our LCSC Liangshan development board is priced at 108 yuan. It is worth buying, easy to use, and trustworthy.
- One-stop service. By purchasing the LCSC Liangshan development board, you can not only acquire embedded knowledge but also learn to design various embedded expansion projects. The JLC group provides a wealth of educational resources and leverages the complete industrial chain of JLC to assist students in completing the design of a comprehensive electronic product project. This includes PCB design, component procurement, PCB fabrication, and 3D printing. Through our open-source platform, you can connect with electronics enthusiasts worldwide, exchange ideas, learn embedded development and debugging techniques, enhance your practical skills, and uncover the mysteries and marvels of embedded systems.
Introduction to Development Board Hardware Parameters
Basic Hardware Parameters of LCSC Liangshan Development Board | |
CPU and Flash Features | Up to 240MHz
Flash up to 1024K SRAM up to 512K |
On-chip Peripheral Characteristics | Up to 3 12-bit ADCs;
Up to 2 12-bit DACs; Up to 8 general-purpose 16-bit timers, 2 basic timers and 2 enhanced timers; Up to 6 SPI, 3 I2C, 4 USART, 2 I2S, 2 CAN, 1 USBFS+HS, 1 ETH, 1 SDIO, 1 Camera, 1 IPA, 1 EXMC/SDRAM |
Board Features | Using TYPE-C, USB provides 5V power supply
It leads to the SWD & serial port debugging interface, and is equipped with a DAPlink emulator to facilitate program download simulation and serial port debugging. On-board RGB565 and 8080 parallel interfaces and external SDRAM expansion facilitate screen clicking. Onboard USB2.0 FS/HS. It leads to 68 programmable IOs to facilitate project expansion. |
Development Board Peripheral Resources
Onboard Resources |
|
User LED Light | GPIO output experiment, timer experiment, DAC experiment. |
User Buttons | GPIO input experiment, external interrupt experiment. |
RGB565 | Screen display experiments, LVGL and other common graphics library experiments. |
8080 Parallel Port | Screen display experiments, LVGL and other common graphics library experiments. |
SD | SDIO experiment, file system experiment. |
FLASH | SPI experiment, file system experiment. |
USB | Simulation experiments on mouse, keyboard, USB disk, etc. |
W9825G6KH | External SDRAM experiment. |
External Resources |
|
Sensor Module | OV2640 camera, OV7670 camera, temperature and humidity sensor, tracking sensor, light sensor, infrared ranging sensor, optical fingerprint recognition, laser ranging sensor, ultrasonic ranging, microwave radar sensor, three-axis acceleration gyroscope, flame sensor, non-contact Infrared temperature sensor, heart rate sensor, magnetic encoder, high-precision analog-to-digital converter, weighing sensor, smoke sensor, alcohol sensor, methane sensor, natural gas/gas sensor, carbon monoxide sensor, carbon dioxide sensor, hydrogen sensor, air quality sensor, Water temperature sensor, human body infrared sensor, RFID sensing module, air pressure sensor, height sensor, Hall encoder, rotary encoder, water level monitoring sensor, color recognition sensor, pressure sensor, current detection module, raindrop detection sensor, pulse sensor, grayscale Sensors, multi-channel touch switches, etc. |
Communication Module | Ethernet module, GPS+Beidou positioning, Bluetooth module, universal infrared module, NRF wireless transmitter and receiver module, PS2 handle wireless remote control, 2.4G communication module, WIFI module, 4G module, NB IOT module, 485 communication module, 232 communication module, CAN Bus module, GSM SMS module, LoRa communication module, etc. |
Display Module | 0.96-inch monochrome screen, 0.96-inch color screen, 1.14-inch color screen, 1.8-inch color screen, 1.9-inch color screen, 1.47-inch color screen, 1.69-inch color screen, 2.0-inch color screen, 4.3-inch color screen, 8-bit digital tube, multi-channel dot matrix screen, etc. |
Other Modules | Multi-channel analog-to-digital converter, high-precision clock module, RGB lantern, data memory, multi-channel relay, optical fingerprint recognition, DC motor drive module, steering gear, multi-channel steering gear drive module, speech recognition module, speech synthesis broadcast module , high-precision analog-to-digital converters, stepper motor drives, passive buzzers, brushless motors, etc. |
LCSC Liangshan Development Board Features
- Compact Appearance
High cost performance, powerful performance, open source software and hardware.
- Development Environment
Equipped with DAPlink emulator to facilitate program downloading, simulation and serial port debugging;
Download method: 1. SWD download 2. DFU download 3. Serial port download;
JLC provides an online compiler to make it easy to get started. You can begin quickly in 10 minutes without installing and configuring various environments.
- Project-based Learning
One-stop comprehensive learning approach. From hardware circuit design, PCB design, component selection and procurement, software design, software and hardware debugging to project completion standards. Through project-based learning, you will eventually be able to effortlessly and enjoyably replicate those very cool open-source projects, as well as attempt to realize your own innovative and unconventional ideas.
- Meet the Teaching Requirements of Multiple Majors
- Suitable for in-class experimental teaching in embedded courses.
- Applicable for embedded course design and microcontroller course design.
- Suitable for college students’ innovation training projects, electronic design competitions, and other application scenarios.