Reflow soldering directly affects the soldering quality of electronic products in the SMT (Surface Mount Technology) manufacturing process. During reflow soldering, solder ball formation is a common issue. Solder balls not only impact the appearance of the solder joints but can also lead to a series of electronic circuit failures, severely compromising the product’s reliability and lifespan. This article explores the causes of solder ball formation and how optimizing the soldering process, material selection, and PCB design can help reduce solder ball occurrence, ensuring high-quality solder joints.
Definition and Impacts of Solder Balls
Solder balls are metallic spheres formed during the reflow soldering process, typically resulting from uneven solder paste application or improper temperature profiles, causing molten solder to drip or form balls. Solder balls not only affect the appearance of product but can also lead to short circuits, cold solder, and weak solder joints.
Impacts of Solder Balls:
- Short Circuits: Solder balls may form a bridge between adjacent pads, causing short circuits and disrupting the normal operation of the device.
- Cold Solder Joints: Solder balls may prevent proper fusion of solder joint, leading to cold joint and resulting in unreliable electrical connections.
- Product Reliability: Solder balls increase the risk of product failure, potentially causing the entire board to be scrapped or significantly shortening its lifespan.
Causes of Solder Ball Formation:
- Uneven Solder Paste Printing: Inconsistent solder paste thickness or incomplete coverage of solder paste can lead to excess solder in certain areas, resulting in solder ball formation.
- Improper Reflow Temperature Profiles: Rapid or uneven temperature changes during soldering can cause solder ball formation at inappropriate melting points.
- PCB Design Defects: Dense pad layouts or improper size of pads can exacerbate solder ball formation.
Analysis of the Causes of Solder Ball Formation
Improper Reflow Temperature Profile
Temperature control during reflow soldering is critical, as each stage of the temperature profile significantly affects soldering quality. A typical reflow soldering temperature profile is divided into four main stages: preheat, soak, reflow, and cooling. If the temperature increases too quickly or unevenly, the solder paste may over-melt at inappropriate temperatures, leading to solder ball formation.
- Excessive Heating Speed: If the heating speed is too fast, volatile substances in the solder paste can be trapped during the soldering process, causing the solder to form sphere and resulting in solder ball formation.
- Temperature Profile Optimization: To reduce solder balls, the temperature during the preheat stage should gradually increase, the peak reflow temperature should be controlled near the solder paste’s melting point, and excessive temperature differences should be avoided.
Keys to Optimize the Temperature Profile:
- Preheat Stage: Both too low or too high temperatures can affect the wettability of the solder. The temperature should be adjusted based on the characteristics of the solder paste.
- Control of Peak Reflow Temperature: The peak reflow temperature should be controlled to ensure that the maximum melting temperature of the solder paste matches the thermal tolerance of the materials used.
Impact of Solder Paste Composition and Storage Management on Solder Ball Formation
Solder Paste Composition
The content of heavy metals, the type, and formulation of flux in the solder paste affect the melting process and wettability with the PCB surface. The solder paste containing a high level of volatile substances can cause the solder to melt too early, resulting in the formation of spherical solder balls.
Solder Paste Storage and Management
The storage conditions of solder paste significantly impact its performance. When exposed to moisture or improper storage conditions, solder paste is susceptible to environmental humidity, which can degrade its performance and increase the risk of solder ball formation. To ensure optimal performance, the following points are crucial:
- Refrigerated Storage: Solder paste should be stored at the appropriate temperature as recommended by the supplier. Preventing moisture exposure is key to maintaining the performance. Typically, solder paste should be allowed to warm up and be thoroughly mixed before use to restore its ideal viscosity and consistency.
- Moisture Prevention: The lid of the solder paste container should be sealed tightly to prevent moisture ingress. Moisture can negatively affect the rheological properties of the paste and accelerate oxidation of the solder, leading to solder ball formation.
Usage Guidelines for Solder Paste
In production, unused solder paste should not be returned to the original container, as it may have been exposed to air, causing changes in its volatile substance and uneven composition. Reintroducing used paste into the container can cause degradation, affecting print quality and increasing the risk of solder ball formation.
Some images are sourced online. Please contact us for removal if any copyright concerns arise.
Custom Cables: Save 50%+ Avg Cost By JST, Molex, TE Alternatives | Processing Fee Down to $1 Per Piece | No Minimum Order Quantity (MOQ) Required
PCB & PCBA: New Customer Get Coupons Up to $125 | 1 – 32 Layers From $2 /5pcs | PCB Assembly From $8 /5pcs
Front Panels: High-quality Front Panel Acrylic/PET | Front Panel Order Up to 30% Off | Membrane Switch Available Soon