HK
Shenzhen Hangshun Chip Technology Development Co., Ltd. (hereinafter referred to as "Hangshun Chip" or "HK") was established in 2013, with branches and offices in Chengdu and Shanghai. It is committed to the mission of "automotive SoC + high-end MCU supermarket dual strategy, making the Internet of Things smarter and smart life better," and realizing the great vision of "taking HK32MCU as the core and building Hangshun Chip's borderless ecological platform-level enterprise." At present, the company has mass-produced seven process platforms from 8-inch 130nm to 12-inch 40nm for digital/analog hybrid, and more than 100 industrial/ commercial/ automotive-grade, general/ special/ customized 32-bit MCUs from twelve major families such as ARM and RISC-V. Hangshun Chip’s HK32MCU is divided into economical, mainstream, low-energy, high-performance, special and innovative types, and is widely used in automobiles, industry, home appliances, the Internet of Things, etc.